The Shard: a majestic cone of light, fed by our cables

When designing this audacious glass and steel sculpture, the architect Renzo Piano drew his inspiration from church spires and the masts of the majestic ships painted by Canaletto in the 1700s. Lofty and elegant, The Shard towers over the River Thames, reaching a record height of 310 metres.
EN - Stories - Projects & Business - Construction & Infrastructures - Shard - Slide
Id: 3533
Type: text_and_gallery
Url: node/3533


A living work of contemporary art
Not only is this unconventional skyscraper a masterpiece of modern architecture; it is a true vertical city boasting luxury apartments, restaurants, hotels, offices and shops distributed throughout its 92 storeys.


Energy, safety and sustainability
In 2011, Prysmian was chosen to be the exclusive supplier of the cables and components that make up every single electrical circuit in The Shard, as well as its official consultant on choosing the best installation methods.
The solution chosen for this challenging project was AFUMEX Low Smoke Zero Halogen cable: a generation of flame-resistant eco-friendly electrical cable, enclosed in a sheath that reduces smoke emissions and is halogen-free. Should a fire break out, this cable limits the spread of the flames and emits extremely low levels of irritating, corrosive gases.

The time variable
Should a fire break out (particularly in a building the size of a skyscraper, with an incredible number of storeys and a high number of occupants inside), time is an essential variable for everyone: for the occupants who will need to evacuate the skyscraper and the emergency services who will need to put the fire out and provide emergency assistance.
AFUMEX cable ensures that there is more time to evacuate the building and carry out emergency procedures.
The AFUMEX range is one of the Group’s jewels in the crown: it has introduced unprecedented benefits, both as regards fire safety and environmental sustainability.
The Prysmian Group has installed its Fire Resistant and AFUMEX cables in many of the world’s most prestigious and densely populated buildings, where fire safety is an absolute priority.
Project numbers
350 km
of fire-resistant power cable
310 metres
Skyscraper’s height
92
Storeys
View Product - EN - Panel - Construction & Infrastructure
Id: 3473
Type: view_product
Url: node/3473

INNOVATION
The future is closer than you think

OPERATIONS
Inside Prysmian’s new ‘smart-working’ HQ

CONSTRUCTION & INFRASTRUCTURE
Burj Khalifa: sky-high safety

OPERATIONS
Fast Forward. Boosting Operations

ETHICS & SUSTAINABILITY
Talking about sustainability

TRANSPORTATION & MOBILITY
Technology at the service of the rebirth of New York

CONSTRUCTION & INFRASTRUCTURES
The Shard: a majestic cone of light, fed by our cables

ETHICS & SUSTAINABILITY
The true power of sustainability
EN - Stories - Magazine
Id: 3957
Type: panel
Url: node/3957